AXIS#.ZEROV
Description
AXIS#.ZEROV is the velocity threshold for the motor to be considered at zero velocity.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
|
| Renamed from AXIS#.DISVTHRESH | 02-03-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
Rotary: RPM Linear: counts/s, mm/s, µm/s, (custom units)/s See Velocity Units for details. |
|
Range |
Depends on units. See Velocity Range for details. |
|
Default Value |
5 RPM Depends on units. See Velocity Units for details. |
|
Data Type |
Float |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.ZEROV |
0x5002 |
0x4 | DINT | - | - | RW | False |
| AXIS2.ZEROV | 0x5102 | 0x4 | DINT | - | - | RW | False |